variable speed control

Electrical EquipmentElectricity 101

How Do AC Motors and Variable Frequency Drives Work?

Electric motors power everything from tiny electronics to massive industrial pumps. Yet, they all work on the same basic principles. Though AC motors seem ordinary, there are complex activities going on behind the scenes. AC Motors The simplest types of motors are three-phase AC motors. They convert a rotating magnetic field into mechanical rotation. The basic parts of an AC motor are the stator, rotor, bearings, drive shaft, and frame. The supply power is connected to coils of wire that are wrapped around laminated iron cores in the stator; the stationary part of the motor. When the coils of wire

Read More