The Basics of Programmable Logic Controllers
Programmable logic controllers provide automatic control of processes so that very little human intervention is required. Yet, this results in a well-coordinated, repetitive process. These systems automatically start and shut down critical equipment in large and complex manufacturing processes. When in operation, programmable logic controllers ensure that all conditions are met before starting up a certain machine or process. In addition, the PLC continues monitoring the entire system using a variety of sensors. Consequently, this ensures that everything runs as programmed. The PLC will trip if it detects a malfunction or abnormality in any of the monitored parameters. The system
Read more