Commercial Electrical Wiring tips

Electrical SafetyElectricity 101

Tips on Commercial Electrical Wiring

Commercial buildings require special considerations when it comes to electrical wiring. Most commercial buildings do not have the luxury of a wooden frame to run wires through, so other wiring methods must be used. Some of those are discussed below. Conduit A common method of electrical wiring in a commercial setting is by use of conduit. Conduits can be made of a variety of materials including steel, aluminum, or PVC depending on the application. For underground conduit runs or conduit embedded in concrete slabs, PVC conduit is used, as it will not rust or corrode. PVC conduit can also be

Read More