Electrical SafetyElectricity 101

Install an Organized Electric Wiring Layout

If you are working with electricity, it is important to know how to safely install an organized electric wiring layout.  Fires and accidents can be caused by faulty electric wiring layouts, so it’s important to be able to recognize potential hazards and avoid them whenever possible.

Although this job may be best left for an electrician, it is still a good idea to know a bit about the work that needs to be done. This way, you can recognize dangerous situations and supervise electrical work being done in your home. Read on to find out all you need to know about safely installing an organized electric wiring layout.

Organizing an Electric Wiring Layout for Your Home

electric wiring layoutThe electric wiring layout for your home will vary according to what room you are doing the wiring for. In any case, it’s a good idea to draw a diagram of the layout first. The diagram will help you determine what lighting or appliances are needed, where they will be located and what sort of outlets will be necessary for each item.

Next you should determine which tools and electrical supplies you will need. It is always best to overestimate on how many outlets will be necessary for your layout, and to buy more than enough wire to complete your job. Once you have a carefully planned outline of what needs to be done, it’s time to start working on the installation. But first, you should familiarize yourself with a few basic safety tips.

Safety Tips for Electrical Wiring Layout:

electric wiring layoutBecause it is so important to have your electric wiring layout installed safely, here are a few tips you should be aware of during the installation process:

  • Make sure all appliances are kept away from water.
  • Install GFCI’s.  These are devices that will shut off the circuit when it detects that current is flowing through an unintended path like a person or water.
  • Read all directions and owners manuals for all appliances and products being used.
  • Use correctly rated fuses for all applicances.
  • Never run more than three appliances off of one socket.
  • Never run electrical cables under carpet.
  • Keep appliances unplugged if they are not being used.
  • Make sure all appliances and electrical supplies being used are quality items that are in good working order.
  • Never clip the third prong off a plug to make it fit a two-prong outlet. This prong provides the path along which the electric current travels.
  • If you are using old equipment or appliances, make sure they are still up to safety standards and in good working order
  • Check on both outdoor and indoor electrical wiring to make sure they are safe
  • Make sure that all electricity is shut off before starting work on our project.

Of course, it’s important to not only make sure your electric wiring layout is installed safely, but that you are safe while installing it. Be sure to follow all safety precautions while you are working. A careful and safe installation will guarantee that your home has a reliable electric wiring layout for years to come.